1.5 SDSPI Driver Asynchronous - SDSPI Read Write

This example application shows how to use the SDSPI driver in asynchronous mode to perform non-blocking operations on the SD Card Media.

Description

  • The asynchronous mode of the SDSPI driver is configured to use DMA and performs non-blocking read and write operations.
  • This application writes 4KB (4096 bytes) of data starting at the SD Card memory location 0x2000, using the SDSPI driver.
  • The application then reads and verifies the written data.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/sdspi/async/sdspi_read_write/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_l10_xpro.XMPLABX project for SAML10 Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_l10_xpro.X SAML10 Xplained Pro Evaluation Kit

Running the Application

  1. Build and program the application using its IDE
  2. The LED is turned ON when the read data from the SD card matches with the written data
Refer to the following table for LED name: