3.2 Updating the Repositories Using the MCC Content Manager
If a repository is downloaded, the MCC Content Manager will query the tag information of the branch on the PC and what is available on the Web. If the Web has a newer version, the user can update the appropriate repository.
If the user has modified a repository, such as changing a configuration, then the user can clean the repository using the MCC Content Manager and update the repository.
Tip: As internet link strength
and server response speed vary, therefore this step might take some time.