2.5.1 Client in Dual Mode Configuration Does Not Work Unless Host is Enabled

Using the client in Dual mode configuration does not work unless host is enabled: ENABLE set to '1' in Host Control (TWIn.MCTRL) register.

Work Around

1. Ensure that the host is always enabled whenever the client is used in the Dual (separate pins) mode. 2. If host functionality is not needed, use the client in the Combined (same pins) mode.

Affected Silicon Revisions

Rev. A1
X