1.1.1.9 FLEXRAMECC_NoFixCallbackRegister
void FLEXRAMECC_NoFixCallbackRegister(FLEXRAMECC_CALLBACK callback, uintptr_t context)
Summary
Sets the pointer to the function (and it's context) to be called when the given FLEXRAMECC's ECC Not Fixable Error interrupt events occur.
Description
This function sets the pointer to a client function to be called "back" when the given FLEXRAMECC's interrupt events occur. It also passes a context value (usually a pointer to a context structure) that is passed into the function when it is called. The specified callback function will be called from the peripheral interrupt context.
Preconditions
FLEXRAMECC_Initialize must have been called for the associated FLEXRAMECC instance.
Parameters
callback - A pointer to a function with a calling signature defined by the FLEXRAMECC_CALLBACK data type. Setting this to NULL disables the callback feature.
contextHandle - A value (usually a pointer) passed (unused) into the function identified by the callback parameter.
Returns
None
Example
Refer to the description of the FLEXRAMECC_CALLBACK data type for example usage.