1.12 DSU Compute CRC32

This example application demonstrates how to use the DSU Peripheral library to compute 32-bit Cyclic Redundancy Checksum (CRC).

Description

The DSU unit provides support for calculating a 32-bit CRC value for a memory area. This example application computes the 32-bit hardware CRC value using the DSU Peripheral and validates it using a software-calculated CRC value.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/dsu/dsu_crc32_generate/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_d21_xpro.XMPLABX project for SAM D21 Xplained Pro Evaluation Kit
sam_da1_xpro.XMPLABX project for SAM DA1 Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_d21_xpro.XSAM D21 Xplained Pro Evaluation Kit
sam_da1_xpro.XSAM DA1 Xplained Pro Evaluation Kit

Setting Up SAM D21 Xplained Pro Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Setting Up SAM DA1 Xplained Pro Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and Program the application using its IDE
  2. The LED indicates the success or failure:
    • LED is turned ON when the hardware CRC value matched with the software calculated CRC value
    • LED is turned OFF when the hardware CRC value did not match with the software calculated CRC value
The following table provides the LED name: