1.6 Clock Configuration

This example application shows how to configure the clock system to run the device at maximum frequency. It also outputs a prescaled clock signal on a GPIO pin for measurement and verification.

Description

Clock system generates and distributes the clock for the processor and peripherals. This example application shows how to use the clock manager to configure the device to run at the max possible speed. A prescaled clock signal is routed to GPIO pin to measure the frequency and accuracy of the internal device clock.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/clock/clock_config/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_d21_xpro.XMPLABX project for SAM D21 Xplained Pro Evaluation Kit
sam_da1_xpro.XMPLABX project for SAM DA1 Xplained Pro Evaluation Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_d21_xpro.XSAM D21 Xplained Pro Evaluation Kit
sam_da1_xpro.XSAM DA1 Xplained Pro Evaluation Kit

Setting Up SAM D21 Xplained Pro Evaluation Kit

  • Connect an oscilloscope to monitor the PORT pin PB15 (Pin 10 of the EXT2 header)
  • Connect the Debug USB port on the board to the computer using a micro USB cable

Setting Up SAM DA1 Xplained Pro Evaluation Kit

  • Connect an oscilloscope to monitor the PORT pin PB15 (Pin 10 of the EXT2 header)
  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and Program the application using its IDE
  2. Observe a clock of 4 MHz on the clock output pin
  3. LED should be blinking continuously
Refer to the following table for clock output pin and LED name for different boards:
BoardClock Output PinLED Name
SAM D21 Xplained Pro Evaluation KitPB15 (Pin 10 of the EXT2 header)LED0
SAM DA1 Xplained Pro Evaluation KitPB15 (Pin 10 of the EXT2 header)LED0