In-system programming (ISP) uses the target Microchip AVR’s internal SPI (Serial
Peripheral Interface) to download code into the Flash and EEPROM memories. It is not a
debugging interface.
Use the pinout shown in the figure below when designing an application PCB with an AVR
with the SPI interface included.Figure 2-1. SPI Header Pinout
Info: The SPI interface is
often referred to as “ISP” since it was the first in-system programming interface on
Microchip AVR products. Other interfaces are now available for in-system
programming.
Direct Connection to a Standard 6-pin 100-mil SPI Header
Use the included 100-mil 6-pin flat cable to connect directly to a board supporting the
SPI header type. Note the pin-1 marking on the cable, and ensure to line it up with the
pin-1 marking on the AVR Programming Adapter.
Important: The SPI interface is effectively disabled
when the debugWIRE enable fuse (DWEN) is programmed, even if the SPIEN fuse is also
programmed. Issue the ‘disable debugWIRE’ command while in a debugWIRE debugging
session to re-enable the SPI interface. Disabling debugWIRE in this manner requires
that the SPIEN fuse is already programmed. If MPLAB® X IDE or
Microchip Studio fails to disable debugWIRE, it is probably because the SPIEN fuse
is NOT programmed. If this is the case, it is necessary to use a high-voltage
programming interface to program the SPIEN fuse.
Table 2-1. SPI Pin Description
MPLAB® Debugger/Programmer Hardware Tools
SPI Pin Mapping
Pin #
Pin Name
Header Pin #
Name
Description
1
TVPP
2
TVDD
2
VCC
Target voltage reference
3
GND
6
GND
Common ground
4
PGD
1
PDO/MISO
SPI data input pin to the programmer. Connect to the MISO pin on the
target device.
5
PGC
3
SCK
SPI serial clock output
6
TAUX
5
RESET
Target reset control pin
7
TTDI
4
PDI/MOSI
SPI data output pin for the programmer. Connect to the MOSI pin on
the target device.