24.5.1 Enabling the CCI
It is assumed that you are using the MPLAB X IDE to build projects that use the CCI. The widget in the MPLAB X IDE Project Properties is used to enable CCI conformance CCI Syntax in the Compiler category.
If you are not using this IDE, then the command-line option is
-mcci for MPLAB XC16.
Differences
This option has never been implemented previously.
Migration to the CCI
Enable the option.
Caveats
None.