19.3 Using Optimizations
The MPLAB XC32 C Compiler for PIC32A
MCU
supports general, as well as several specific, optimization options (see section Options for Controlling Optimization). In most cases, only
general optimization options (-On) should be used (for details, see
How to Enable Optimization).
The more a compiler optimizes the output code, the further away from the C program the code might become. This is the nature of optimization and is often exasperated by a weakness of debug information to represent these changes. Optimizations tend to:
- convert structures into scalar variables (to remove unused members)
- re-order flow, or duplicate it, for speed improvements
- capture results, or partial results, for re-use later
- remove unreachable code
- remove unused variables or promote an object to a register variable
- remove code that has no externally visible effect
Many of these transformations can make debugging code much more difficult. Some of them can turn a “working” program into something that no-longer executes correctly; typically, this means that the working program is not a well-formed C program and the optimizer has exposed this.