14.2 Function Size Limits
For all devices, the code generated for a function may become arbitrarily large, limited
only by the available program memory. The efficiency of call sequences is determined by the
code memory model. By default, the "small code" model is selected, which results in the
most efficient call sequence. The linker will determine if source and destination are close
enough to permit use of the small code model. If not, a helpful message will suggest that
the "large code" model should be specified in MPLAB X IDE Project
Properties or by using the -mlarge-code command option.
When the large code model is specified, call sequences will be automatically converted to the most efficient form whenever possible by the assembler. This typically occurs when both source and destination are defined in the same compilation unit, and are within range of the more efficient instruction sequence.