1.5.3.1 How The Library Works
The PRIME User PIBs service library offers the PRIME Stack the necessary functions to
handle the user PIBs, which include:
- get user-defined parameters
- set user-defined parameters
- set callbacks
The PRIME Stack uses this interface to access the user PIBs when they are requested via MLME, Serial Profile or PRIME Profile by the user.
This library needs to be initialized, but it does not need to be maintained periodically.
This library does not include storage. Users are responsible for adding and storing their own PIBs.
Currently, there are user PIBs related to the reset handling, which are stored in the GPBRs by the PRIME Reset Handler service library (see Reset Handler Service).
| PIB | ID | Contents |
|---|---|---|
| PIB_USER_RESET_INFO | 0xF000 | number of resets + reset type |
| PIB_USER_PC | 0xF001 | PC |
| PIB_USER_LR | 0xF002 | LR |
| PIB_USER_PSR | 0xF003 | PSR |
| PIB_USER_HFSR | 0xF004 | HFSR |
| PIB_USER_CFSR | 0xF005 | CFSR |
| PIB_USER_R0 | 0xF006 | R0 |
| PIB_USER_R1 | 0xF007 | R1 |
| PIB_USER_R2 | 0xF008 | R2 |
| PIB_USER_R3 | 0xF009 | R3 |
| PIB_USER_R12 | 0xF00A | R12 |