1.5.1.2 Using The Library
The PRIME Storage service library is called to read/write persistent data from/to non-volatile memory.
The following example illustrates how the Storage service can be used.
Example of PRIME Storage library usage
#include <string.h>
#include "app.h"
#include "service/storage/srv_storage.h"
#include "bsp/bsp.h"
typedef struct {
uint16_t key;
uint8_t eui48[6];
} PRIME_MAC_EUI48;
#define MAC_CONFIG_KEY 0xAA55
void APP_Initialize ( void )
{
PRIME_MAC_EUI48 macEUI48;
SRV_STORAGE_GetConfigInfo(SRV_STORAGE_TYPE_MAC_INFO, sizeof(macEUI48), &macEUI48);
if (macEUI48.key == MAC_CONFIG_KEY)
{
LED_GREEN_On();
}
else
{
LED_BLUE_On();
}
}
void APP_SetEUI48(uint8_t* eui48)
{
PRIME_MAC_EUI48 macEUI48;
macEUI48.key = MAC_CONFIG_KEY;
memcpy(macEUI48.eui48, eui48, 6);
SRV_STORAGE_SetConfigInfo(SRV_STORAGE_TYPE_MAC_INFO, sizeof(eui48), &eui48);
}