| PIB_MTP_MAC_EUI_48 | 0x8100 | 6 bytes | - | MAC address. |
| PIB_MAC_PLC_STATE | 0x8101 | 1 byte | - | PRIME PLC state:- 0: SN
disconnected
- 1: SN
detection
- 2: SN
registering
- 3: SN
operative
- 4: BN
|
| PIB_MAC_SERVICE_STATE | 0x8102 | 1 byte | - | Service Node state:- 0: SN disconnected
- 1: SN registering
- 2: SN terminal
- 3: SN unregistering
- 4: SN promoting
- 5: SN switch
- 6: SN demoting
- 7: SN roaming
|
| PIB_MAC_REG_RSS | 0x8103 | 1 byte | 0 - 255 | Attenuation level to send REG and PNPDU messages in a SN in PRIME
v1.3.6. |
| PIB_MAC_ACTION_CFP_LENGTH | 0x810D | 2 bytes | 0 - 128 | Set CFP length in symbols in MAC certification mode in a
BN. |
| PIB_MAC_ACTION_BCN_SLOT_COUNT | 0x810E | 1 byte | 1 - 4 | Change the number of beacon slots per frame in MAC certification
mode in a BN in PRIME v1.3.6. |
| PIB_MAC_ALV_MIN_LEVEL | 0x810F | 1 byte | 1 - 64 | Set the minimum level of the node to add independent records to
the alive response message (64 = default handling) in a BN in PRIME
v1.4. |
| PIB_MAC_ACTION_FRAME_LENGTH | 0x8110 | 1 byte | 0 - 3 | Frame length in the present superframe of a BN in PRIME v1.4:- 0: 276
symbols
- 1: 552
symbols
- 2: 828
symbols
- 3: 1104
symbols
|
| PIB_CERTIFICATION_MODE | 0x8120 | 1 byte | 0 - 3 | Certification mode:- 0: no
certification mode
- 1: PHY
certification for 1.3
- 2: MAC
certification
- 3: PHY
certification for 1.4
|
| PIB_CERTIFICATION_SEND_MSG | 0x8121 | Array | - | Send message in PHY certification mode. See description below
this table. |
| PIB_MTP_MAC_WRITE_SNA | 0x8123 | 6 bytes | - | Write SNA in MTP mode in a BN. |
| PIB_MAC_ACTION_ARQ_WIN_SIZE | 0x8124 | 1 byte | 1 - 32 | Change the ARQ window size in MAC certification mode in a
BN. |
| PIB_MAC_INTERNAL_SW_VERSION | 0x8126 | 4 bytes | - | MAC internal software version. |
| PIB_CERT_MIN_LEVEL_TO_REG | 0x8130 | 1 byte | 0 - 63 | Minimum level where the SN can register in PRIME v1.4. |
| PIB_BCN_SLOTS_BUSY | 0x8131 | 1 byte | 0 - 128 | Number of used beacon slots in a BN in PRIME v1.3.6. |
| PIB_MAC_ACTION_MGMT_MUL_SEND_DATA | 0x8132 | 3 bytes | - | Send multicast data through the Management connection using the
given length (first 2 bytes) and priority (third byte) in a BN in
PRIME v1.4. |
| PIB_MAC_ACTION_BCN_TX_SCHEME | 0x8133 | 1 byte | 0 - 2 | Change the beacon modulation in MAC certification mode in a BN in
PRIME v1.4:- 0:
DBPSK_CC
- 1:
R_DQPSK
- 2:
R_DBPSK
|
| PIB_MAC_ACTION_ALV_TYPE | 0x8134 | 1 byte | 0 - 1 | Change the ALV mode in a BN in PRIME v1.4:- 0: 1.4 ALV
mode
- 1: 1.3 ALV
mode
|
| PIB_MAC_CHN_SCANNING_MODE | 0x8135 | 1 byte | 0 - 3 | Change the channel scanning mode in a SN in PRIME v1.4.
- 0: start
with random channel and scan in ascending order
- 1: start
with random channel and scan in descending order
- 2: start
with next registered channel and scan in ascending
order
- 3: start
with previous registered channel and scan in descending
order
|
| PIB_MAC_ACTION_CFG_BCN_SWITCH_RATE | 0x8136 | 1 byte | 0 - 5 | Transmission frequency of the beacon in switches (PRO.FRQ) in a
BN in PRIME v1.4. |
| PIB_MAC_ACTION_CFG_SEC_PROF | 0x8137 | 1 byte | 0 - 2 | Security profile to be used in the network in a BN in PRIME
v1.4. |
| PIB_MAC_SEC_DUK_BN | 0x8140 | 22 bytes | - | DUK for the indicated service node. The first six bytes
correspond to the MAC address of a service node. The following bytes
are its DUK. In a BN in PRIME v1.4. |
| PIB_MAC_SEC_PROFILE_USED | 0x8141 | 1 byte | 0 - 2 | Security profile used in the network where the Service Node is
registered in PRIME v1.4. |
| PIB_MAC_SEC_OLD_SWK_TIME | 0x8142 | 2 bytes | 0 - 10800 | Validity time (in seconds) of the old SWK during a key update
process in a BN in PRIME v1.4. |
| PIB_MAC_WHITELIST | 0x8150 | - | - | List of MAC addresses of nodes which are allowed to register in a
BN. |
| PIB_MAC_WHITELIST_ENABLED | 0x8151 | 1 byte | 0 - 1 | Whitelist status [0: disabled, 1: enabled] in a BN. |
| PIB_MAC_ACTION_CLEAR_NWK_STRUCTURE | 0x8152 | 1 byte | 0 - 1 | Clear network structure in a BN. |