1.2.4 PRIME_Tasks Function
C
void PRIME_Tasks ( SYS_MODULE_OBJ object )
Summary
Maintains the PRIME Stack State Machine.
Description
This routine maintains the PRIME Stack State Machine.
Precondition
PRIME_Initialize routine must have been called before, and its returned object used when calling this function.
Parameters
| Parameters | Description |
|---|---|
| object | Identifier for the object instance |
Returns
None.
Example
PRIME_STACK_INIT initData;
SYS_MODULE_OBJ sysObjPrime;
sysObjPrime = PRIME_Initialize(PRIME_INDEX_0, (SYS_MODULE_INIT *)&initData);
while (true)
{
PRIME_Tasks(sysObjPrime);
}
Remarks
This routine must be called periodically.