1.2.5 PRIME_Restart Function

C

void PRIME_Restart
(
  uint32_t *primePtr,
  uint8_t version
)

Summary

Restarts the PRIME Stack from a different location.

Description

This routine restarts the PRIME Stack from a different location.

Precondition

PRIME_Initialize routine must have been called before.

Parameters

ParametersDescription
primePtrPointer to the PRIME API
versionPRIME version to run

Returns

None.

Example

PRIME_STACK_INIT initData;

PRIME_Initialize(PRIME_INDEX_0, (SYS_MODULE_INIT *)&initData);

const PRIME_API *primeApiPtr = PRIME_SN_FWSTACK13_ADDRESS;
PRIME_Restart((uint32_t *)primeApiPtr, PRIME_VERSION_1_3);

Remarks

None.