1.4.3.33 PAL_GetConfiguration Function

C

uint8_t PAL_GetConfiguration(uint16_t pch, uint16_t id, void *val,
    uint16_t length);

Summary

Get a PHY attribute.

Description

This function is used to get a PHY attribute from the selected medium.

Precondition

The PAL_Initialize function should have been called before calling this function.

Parameters

ParametersDescription
pchPhysical channel
idIdentifiers requested from the MAC layer
valOutput parameter value
lengthLength of the parameter

Returns

  • PAL_CFG_SUCCESS: If successful
  • PAL_CFG_INVALID_INPUT: If unsuccessful

Example

 
    uint8_t result=PAL_CFG_SUCCESS;
    uint16_t id=PAL_ID_CFG_ATTENUATION;
    void val=0;
    uint16_t len=1;
    uint16_t pch = 16;

    result = PAL_GetConfiguration(pch, id, &val, len);

Remarks

None.