1.4.3.34 PAL_SetConfiguration Function
C
uint8_t PAL_SetConfiguration(uint16_t pch, uint16_t id, void *val,
uint16_t length);
Summary
Set PHY attribute.
Description
This function is used to set a PHY attribute in the selected medium.
Precondition
The PAL_Initialize function should have been called before calling this function.
Parameters
| Parameters | Description |
|---|---|
| pch | Physical channel |
| id | PHY attribute identifier |
| val | Input parameter value |
| length | Length of the parameter |
Returns
- PAL_CFG_SUCCESS: If successful
- PAL_CFG_INVALID_INPUT: If unsuccessful
Example
uint8_t result=PAL_CFG_SUCCESS;
uint16_t id=PAL_ID_CFG_ATTENUATION;
void val=2;
uint16_t len=1;
uint16_t pch = 16;
result = PAL_SetConfiguration(pch, id, &val, len);
Remarks
Not available for PHY Serial.