1.5.3.4.4 SRV_USER_PIB_GetRequestCbRegister Function

C

void SRV_USER_PIB_GetRequestCbRegister(SRV_USER_PIB_GET_REQUEST_CALLBACK callback);

Summary

Register a function to be called to get the requested user PIB.

Description

This routine allows a client to register an event handling function to be called when a requested user PIB is returned.

Parameters

ParametersDescription
callbackPointer to the callback function

Returns

None.

Example

static void APP_GetRequestHandler(uint8_t getResult, uint16_t pibAttrib,
                                  void *pibValue, uint8_t pibSize)
{
    if (getResult == true)
    {
        ...
    }
}

int main(void)
{
    SRV_USER_PIB_Initialize();

    SRV_USER_PIB_GetRequestCbRegister(APP_GetRequestHandler);
}

Remarks

None.