1.3.5.1.7 PRIME_API_Open Function

C

void PRIME_API_Initialize(void)

Summary

Opens the PRIME Library.

Description

This routine opens the PRIME Library.

Precondition

The PRIME_API_Initialize function should have been called before calling this function.

Parameters

None.

Returns

None.

Example

PRIME_API_INIT init;

init.palIndex = PRIME_PAL_INDEX;
init.halApi = (HAL_API*)&halApi;
init.mngPlaneUsiPort = PRIME_MNG_PLANE_USI_INDEX;

PRIME_API_Initialize(&init, false, PRIME_VERSION_1_4);
    
PRIME_API_Open();

Remarks

This routine is normally not called directly by an application. The PRIME application must use the function located in the PRIME API.