1.3.5.1.6 PRIME_API_Initialize Function

C

void PRIME_API_Initialize
(
    PRIME_API_INIT *init, 
    bool isRestart, 
    uint8_t primeVersion
)

Summary

Initializes the PRIME Library.

Description

This routine initializes the PRIME Library.

Precondition

None.

Parameters

ParametersDescription
initPointer to the init data structure containing any data necessary to initialize the module
isRestartFlag to indicate if this is a restart
primeVersionPRIME version to run

Returns

None.

Example

PRIME_API_INIT init;

init.palIndex = PRIME_PAL_INDEX;
init.halApi = (HAL_API*)&halApi;
init.mngPlaneUsiPort = PRIME_MNG_PLANE_USI_INDEX;

PRIME_API_Initialize(&init, false, PRIME_VERSION_1_4);

Remarks

This routine is normally not called directly by an application. The PRIME application must use the function located in the PRIME API.