2.4 Creating a New Harmony Project

  1. Open the MPLAB X IDE.
  2. Create a New Project by clicking the New Project icon or by selecting File>New Project.
  3. In the New Project window select Application Project(s) and click Next.
    Figure 2-1. New Project
  4. Select the device. For this example, select PIC32CX2051MTG128. Then, click Next.
    Figure 2-2. Device Selection
  5. Select the compiler toolchain and click Next.
    Figure 2-3. Compiler Toolchain Selection
  6. Fill in the needed project information as follows:
    • Name: Enter Project Name (for example, MyFirstPRIMEapp)
    • Location: Enter a valid path to store the application project
    • Folder: Selecting the above fields auto populates the Project Folder
    • Mark Set as main project and Open MCC on Finish
    • Click Finish
    Figure 2-4. Project Information
  7. The above step will open MCC Project Graph.
    Figure 2-5. MCC Project Graph