3.3.3.7 DEF_ANTI_TCH_DRIFT_RATE
This parameter works in the same way as DEF_TCH_DRIFT_RATE - but in the opposite direction.
When the signal value is smaller than the reference, this value defines the rate at which the sensor reference value should be adjusted towards the change in signal value. Away from Touch Drift Rate value is scaled by 200 ms. If Away from Touch Drift Rate is 10 , then the drift period is 10 x 200 ms = 2s . Every two seconds, the reference value will be decremented by 1 until it is equal to the signal value.
Parameter | Range |
DEF_ANTI_TCH_DRIFT_RATE | 0 to 255 Units: 200ms Eg - 5u = 1second |