3.3.3.9 DEF_REBURST_MODE
Under various conditions (like Calibration, Detect Integration, Recalibration), additional touch measurements need to be performed to confirm an activity. This parameter defines how the re-bursting (additional touch measurements) happens. It is recommended to use the default value in order to get faster response time. If re-burst is disabled, then the additional measurements are done at normal scan rate which may increase the response time. If re-burst all active sensors are used, all the active sensors are measured irrespective of their state which again affects the response time. If REBURST_UNRESOLVED is used, then additional measurements are performed only on sensors which are in the process of calibration/ filter in/ filter out and AKS groups.
Parameter | Range |
DEF_REBURST_MODE | REBURST_NONE / REBURST_UNRESOLVED / REBURST_ALL |
The following figures show how each reburst is done.