3.3.6.1 TAP_RELEASE_TIMEOUT
The TAP_RELEASE_TIMEOUT parameter limits the amount of time allowed between the initial finger press and the liftoff. Exceeding this value will cause the firmware to not consider the gesture as a tap gesture. TAP_RELEASE_TIMEOUT should be lesser than the TAP_HOLD_TIMEOUT and SWIPE_TIMEOUT.
Unit: x10 ms
Example: If TAP_RELEASE_TIMEOUT is configured as 3, then the user should finish tapping within 30 ms to qualify the gesture as tap.
Parameter | Range |
TAP_RELEASE_TIMEOUT | 3 to 255 |