3.3.3.9 DEF_REBURST_MODE

Under various conditions (like Calibration, Detect Integration, Recalibration), additional touch measurements need to be performed to confirm an activity. This parameter defines how the re-bursting (additional touch measurements) happens. It is recommended to use the default value to get a faster response time. If re-burst is disabled, then the additional measurements are done at a normal scan rate which may increase the response time. If re-burst all active sensors are used, all the active sensors are measured irrespective of their state, which again affects the response time. If REBURST_UNRESOLVED is used, then additional measurements are performed only on the sensors which are in the process of calibration/filter in/filter out and AKS groups.

ParameterRange
DEF_REBURST_MODEREBURST_NONE / REBURST_UNRESOLVED / REBURST_ALL

The following figure show how each re-burst is done.