2.3.3.5 DEF_ANTI_TCH_RECAL_THRSHLD
This parameter is complementary to DEF_ANTI_TCH_DET_INT. Where DEF_ANTI_TCH_DET_INT acts as the confirmation, this parameter acts as the threshold. If the touch delta is more than "Anti Touch Recal Threshold" on the negative side for DEF_ANTI_TCH_DET_INT times, then the sensor is recalibrated. This parameter is configured as a percentage of the Sensor Threshold.
| Parameter | Range |
| DEF_ANTI_TCH_RECAL_THRSHLD | RECAL_100/ RECAL_50 / RECAL_25 / RECAL_12_5 / RECAL_6_25 |