6.1.2.4 DIAG_SRAM_MARCH_ALT_CLK_FRQ_ENABLED
#define DIAG_SRAM_MARCH_ALT_CLK_FRQ_ENABLED 1
Decides if an alternative main clock frequency will be used when calling DIAG_SRAM_MarchCMinus in DIAG_SRAM_MarchStartup(). If the macro is not zero, it enables the use of an alternative main clock frequency given by DIAG_SRAM_MARCH_ALT_CLK_FRQ. The main clock frequency is set back to the default reset value before returning from DIAG_SRAM_MarchStartup(). Setting the macro to zero results in using the default frequency during the execution of the SRAM March test at start-up.