4.1.3 Can I Install More Than One Version of the Same Compiler?
Yes. The compilers and installation process have been designed to allow you to have more than one version of the same compiler installed. Compilers should be installed into a directory that is named according to the compiler version. This is reflected in the default directory specified by the installer. For example, the MPLAB XC-DSC compilers v3.00 and v3.10 would typically be placed in separate directories, as shown below:
C:/Program Files/Microchip/xc-dsc/v3.00/
C:/Program Files/Microchip/xc-dsc/v3.10/
See also: 4.2.3 How Can I Select Which Compiler Version to Build With?