11.4.2 Define Variables Within an External Space

The external space attribute is also used to assign individual variables to the space. This requires that the memory space declaration to be present. Given the declarations in the previous subsection, the following variable declarations can be made:

__external__ int external_array[256]

__attribute__((space(external(external_memory))));

external_array will be allocated in the previous declared memory external_memory.

Note that the variable has been qualified with a new type qualifier __external__. When attached to a variable or pointer target, it instructs the compiler to generate the correct sequence to access these objects.

Once an external memory variable has been declared, it may be accessed using normal C/C++ syntax. The compiler will generate code to access the variable via special helper functions that the programmer must define. These are covered in the next subsection.