2.1 Installing the UHF Transceiver Z Wave Library (Z-Wave) Release Package

To download UHFTransceiverZWaveLibrary_REL_Vxx.exe, go to ATA8510.

The following are the steps to install the Z-Wave library:
  1. Run the UHFTransceiverZWaveLibrary_REL_Vxx.exe executable file to start the installation procedure. Click I Agree to continue.
    Note: ‘xx’ in the release package executable file name specifies the version of the release package, and it varies according to the library updates. For example, in this scenario, it is 1.0.
    Figure 2-1. Z-Wave Library Installation
  2. Click Next to continue.
    Figure 2-2. Z-Wave Library Installation
  3. The tool creates Z-Wave project folder under C:\Microchip\UHFTransceiverZWaveLibrary_REL_V10 (default path). Click Install to continue with the installation procedure.
    Figure 2-3. Z-Wave Library Installation
  4. Click Close to complete the installation procedure.
    Figure 2-4. Z-Wave Library Installation