4.1.7.3.12 ZCL_SetReportableChange Function
C
ZCL_Status_t ZCL_SetReportableChange(Endpoint_t endpointId, ClusterId_t clusterId, uint8_t clusterSide, ZCL_AttributeId_t attrId, uint8_t attrType, uint8_t *repChange);Description
Finds an attribute in ZCL and rewrites its reportable change value by the new one
\ingroup zcl_common
If the reportable change value of an attribute is set to a non-zero value, using this function, the stack checks how much the attribute has changed each time a new value is set to it. The current (just set) value is compared with the last reported value, and if the absolute difference is greater than the reportable change value a new report is generated and sent to the air.
Parameters
| Param | Description |
|---|---|
| endpointId | endpoint on which cluster is registered |
| clusterId | cluster unique identifier |
| clusterSide | determs the cluster's side (client or server) |
| attrId | attribute unique identifier |
| attrType | type of the attribute to be set |
| repChange | pointer to reportable change value to be set |
Returns
ZCL status of operation.