4.3.1.4.1 AVR® XMEGA® Special Considerations
OCD and Clocking
When the MCU enters Stopped mode, the OCD clock is used as MCU clock. The OCD clock is either the JTAG TCK if the JTAG interface is being used, or the PDI_CLK if the PDI interface is being used.
I/O Modules in Stopped Mode
In contrast to earlier Microchip megaAVR devices, in XMEGA, the I/O modules are stopped in Stop mode. This means that USART transmissions will be interrupted and timers (and PWM) will be stopped.
Hardware Breakpoints
There are four hardware breakpoint comparators - two address comparators and two value comparators. They have certain restrictions:
-
All breakpoints must be of the same type (program or data).
-
All data breakpoints must be in the same memory area (I/O, SRAM, or XRAM).
-
There can only be one breakpoint if the address range is used.
Here are the different combinations that can be set:
-
Two single data or program address breakpoints.
-
One data or program address range breakpoint.
-
Two single data address breakpoints with single value compare.
-
One data breakpoint with address range, value range, or both.
MPLAB X IDE and Microchip Studio will tell you if the breakpoint cannot be set, and why. Data breakpoints have priority over program breakpoints if software breakpoints are available.
JTAGEN Fuse
The JTAG interface is enabled using the JTAGEN fuse, which is programmed by default. This allows access to the JTAG programming interface.
If the JTAGEN fuse is programmed, the JTAG interface can still be disabled in firmware by setting the JTAG disable bit in the MCU Control Register. This will render code un-debuggable and should not be done when attempting a debug session. If such code is already executing on the Microchip AVR device when starting a debug session, the MPLAB ICD 5 will assert the RESET line while connecting. If this line is wired correctly, it will force the target AVR device into Reset, thereby allowing a JTAG connection.
If the JTAG interface is enabled, the JTAG pins cannot be used for alternative pin functions. They will remain dedicated JTAG pins until either the JTAG interface is disabled by setting the JTAG disable bit from the program code, or by clearing the JTAGEN fuse through a programming interface.
Selecting the “use external reset” checkbox, in both the programming dialog and debug options dialog in Microchip Studio, allows the MPLAB ICD 5 to assert the RESET line. This also re-enables the JTAG interface on devices, which are running code that disables the JTAG interface by setting the JTAG disable bit.
Debugging with Sleep for ATxmegaA1 rev H and Earlier
A bug existed on early versions of ATxmegaA1 devices that prevented the OCD from being enabled while the device was in certain sleep modes. There are two work-arounds to re-enable OCD:
- Go into the MPLAB ICD 5. Options in the Tools menu and enable “Always activate external Reset when reprogramming device.”
- Perform a chip erase.
The sleep modes that trigger this bug are:
- Power-Down
- Power-Save
- Standby
- Extended Standby