1.7 CMP Configurable Reference
This example application shows how to use the CMP Peripheral library to compare voltage level on the negative input with the internal configurable reference voltage.
Description
The peripheral named comparator voltage reference (CVR) or CDAC can be used by the CMP peripheral. It generates a voltage that can be connected internally to the +ve input of the any of the comparators in the device. This allows to set flexible compare voltages.
Downloading and building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/cmp/cmp_configurable_reference/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | MPLABX project for PIC32MM USB Curiosity board |
Setting up the hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | PIC32MM USB Curiosity board |
Setting up PIC32MM USB Curiosity Board
- To run the demo, the following additional hardware are required:
- Connect micro USB cable to the 'USB1' on the board to the computer
- Install an USB UART click board on to the mikroBUS socket J4
- Connect mini USB cable to the USB UART click board and PC
- RB0 (C2INB) on J12 is the
negative input, connect it to a voltage below the reference voltage (~1.6V
from CVR peripheral) to trigger interruptNote: Ensure that the series resistors on the mikroBUS headers are of value 0 Ohms
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
- Connect to the "USB to UART" COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application project using its IDE
- Following message is output on console: