1.22 TMR Periodic Interrupt
This example demonstrates how to use the TMR module in timer mode to generate periodic interrupt.
Description
The TMR module generates periodic interrupt on 1 second period match. The LED is toggled in the interrupt handler to indicate periodic callback. Two TMR modules are used to form a 32-bit timer.
Downloading and building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/tmr/tmr_timer_mode/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | MPLABX project for PIC32MM USB Curiosity board |
Setting up the hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32mm_usb_curiosity.X | PIC32MM USB Curiosity board |
Setting up PIC32MM USB Curiosity Board
- Connect micro USB cable to the 'USB1' connector on the board to the computer
Running the Application
- Build and program the application project using its IDE
- On successful execution, LED starts blinking
Following table provides the LED name:
| Board | LED Name |
|---|---|
| PIC32MM USB Curiosity board | LED1 |