1.2.1.1.2.7 "sxops" interface for EC J-PAKE computations.
Simpler functions to perform public key crypto operations. Included directly in some interfaces (like sxbuf or OpenSSL engine). The functions take input operands (large integers) and output operands which will receive the computed results.
Operands have the "sx_op" type. The specific interfaces (like sxbuf) define the "sx_op" type.
@file
ECJPAKE_HEADER_FILE Macro
C
#define ECJPAKE_HEADER_FILE
/ Copyright (c) 2020 Silex Insight sa SPDX-License-Identifier: BSD-3-Clause
Make sure the application is compatible with SilexPK API version **/
SX_PK_API_ASSERT_COMPATIBLE(1, 3);
struct sx_pk_ecurve;
sx_pk_point Function
C
struct sx_pk_point {@addtogroup SX_PK_SXOPS_ECJPAKE
@{
Curve generator point for sx_ecjpake_verify_zkp() or sx_ecjpake_verify_zkp_go() */
Affine point parameter group
This structure is used for point values which are stored in two consecutive locations (x and y). struct sx_pk_point { sx_op x; /< x-coordinate / sx_op y; /< y-coordinate / };
Asynchronous EC J-PAKE proof generation
Start a EC J-PAKE proof generation operation on the accelerator and return immediately.
@remark When the operation finishes on the accelerator, call sx_async_generate_zkp_end()
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
v Random input (< n)
Parameters
x Exponent
Parameters
h Hash digest Truncation or padding should be done by user application @return Acquired acceleration request for this operation static inline struct sx_pk_dreq sx_ecjpake_generate_zkp_go( const struct sx_pk_ecurve curve, const sx_op v, const sx_op x, const sx_op h) { struct sx_pk_dreq pkreq; struct sx_pk_inops_ecjpake_generate_zkp inputs; pkreq = SX_PK_ACQUIRE_REQ(curve->cnx, SX_PK_CMD_ECJPAKE_GENERATE_ZKP); if (pkreq.status) return pkreq; pkreq.status = SX_PK_LIST_ECC_INSLOTS(pkreq.req, curve, 0, (struct sx_pk_slot )&inputs); if (pkreq.status) return pkreq; int opsz = SX_PK_GET_OPSIZE(pkreq.req); SX_PK_OP2MEM(v, inputs.v.addr, opsz); SX_PK_OP2MEM(x, inputs.x.addr, opsz); SX_PK_OP2MEM(h, inputs.h.addr, opsz); SX_PK_RUN(pkreq.req); return pkreq; }
Finish asynchronous (non-blocking) EC J-PAKE proof generation.
Get the output operands of the EC J-PAKE proof generation and release the reserved resources. @pre The operation on the accelerator must be finished before calling this function.
Parameters
req The previously acquired acceleration request for this operation
Parameters
r The resulting value static inline void sx_ecjpake_generate_zkp_end( sx_pk_accel req, sx_op r) { sx_async_finish_single(req, r); }
Perform an EC J-PAKE proof generation
The proof generation has the following steps: | Param | Description | |:----- |:----------- |
| 1. r = (v | (x h)) % n
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
v Random input (< n)
Parameters
x Exponent
Parameters
h Hash digest Truncation or padding should be done by user application
Parameters
r The result @return ::SX_OK @return ::SX_ERR_OUT_OF_RANGE @return ::SX_ERR_POINT_NOT_ON_CURVE @return ::SX_ERR_NOT_INVERTIBLE @return ::SX_ERR_UNKNOWN_ERROR @return ::SX_ERR_BUSY @return ::SX_ERR_NOT_IMPLEMENTED @return ::SX_ERR_OPERAND_TOO_LARGE @return ::SX_ERR_PLATFORM_ERROR @return ::SX_ERR_EXPIRED @see sx_async_ecjpake_generate_zkp_go(), sx_async_ecjpake_generate_zkp_end() for an asynchronous version static inline int sx_ecjpake_generate_zkp( const struct sx_pk_ecurve curve, const sx_op v, const sx_op x, const sx_op h, sx_op r ) { uint32_t status; struct sx_pk_dreq pkreq; pkreq = sx_ecjpake_generate_zkp_go(curve, v, x, h); if (pkreq.status) return pkreq.status; status = SX_PK_WAIT(pkreq.req); sx_ecjpake_generate_zkp_end(pkreq.req, r); return status; }
Asynchronous EC J-PAKE proof verification
Start an EC J-PAKE proof verification operation on the accelerator and return immediately. @remark When the operation finishes on the accelerator, call sx_ecjpake_verify_zkp_end()
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
v Point on the curve
Parameters
x Point on the curve
Parameters
r Proof to be verified
Parameters
h Hash digest
Parameters
g Point on the curve (Optional, pass SX_PT_CURVE_GENERATOR to use the curve generator point) Truncation or padding should be done by user application @return Acquired acceleration request for this operation static inline struct sx_pk_dreq sx_ecjpake_verify_zkp_go( const struct sx_pk_ecurve curve, const struct sx_pk_point v, const struct sx_pk_point x, const sx_op r, const sx_op h, const struct sx_pk_point g) { struct sx_pk_dreq pkreq; struct sx_pk_inops_ecjpake_verify_zkp inputs; pkreq = SX_PK_ACQUIRE_REQ(curve->cnx, SX_PK_CMD_ECJPAKE_VERIFY_ZKP); if (pkreq.status) return pkreq; pkreq.status = SX_PK_LIST_ECC_INSLOTS(pkreq.req, curve, 0, (struct sx_pk_slot )&inputs); if (pkreq.status) return pkreq; int opsz = SX_PK_GET_OPSIZE(pkreq.req); sx_pk_op2mem(v->x, inputs.xv.addr, opsz); sx_pk_op2mem(v->y, inputs.yv.addr, opsz); sx_pk_op2mem(x->x, inputs.xx.addr, opsz); sx_pk_op2mem(x->y, inputs.yx.addr, opsz); sx_pk_op2mem(r, inputs.r.addr, opsz); sx_pk_op2mem(h, inputs.h.addr, opsz); if (g != SX_PT_CURVE_GENERATOR) { sx_pk_op2mem(g->x, inputs.xg2.addr, opsz); sx_pk_op2mem(g->y, inputs.yg2.addr, opsz); } else { sx_pk_write_curve_gen(pkreq.req, curve, inputs.xg2, inputs.yg2); } SX_PK_RUN(pkreq.req); return pkreq; }
Finish asynchronous (non-blocking) EC J-PAKE proof verification.
Finishes the EC J-PAKE proof verification and releases the reserved resources. @pre The operation on the accelerator must be finished before calling this function.
Parameters
req The previously acquired acceleration request for this operation static inline void sx_ecjpake_verify_zkp_end( sx_pk_accel req ) { sx_pk_release_req(req); }
Synchronous EC J-PAKE proof verification
Start an EC J-PAKE proof verification operation on the accelerator and return immediately. The proof verification has the following steps: 1. ( (G r) + (X h) ) ?= V In case of a comparison failure SX_ERR_INVALID_SIGNATURE shall be returned. @remark When the operation finishes on the accelerator, call sx_ecjpake_verify_zkp_end()
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
v Point on the curve
Parameters
x Point on the curve
Parameters
r Proof to be verified
Parameters
h Hash digest
Parameters
g Point on the curve (Optional, pass SX_PT_CURVE_GENERATOR to use the curve generator point) Truncation or padding should be done by user application @return ::SX_OK @return ::SX_ERR_INVALID_SIGNATURE @return ::SX_ERR_OUT_OF_RANGE @return ::SX_ERR_POINT_NOT_ON_CURVE @return ::SX_ERR_NOT_INVERTIBLE @return ::SX_ERR_UNKNOWN_ERROR @return ::SX_ERR_BUSY @return ::SX_ERR_NOT_IMPLEMENTED @return ::SX_ERR_OPERAND_TOO_LARGE @return ::SX_ERR_PLATFORM_ERROR @return ::SX_ERR_EXPIRED @see sx_async_ecjpake_verify_zkp_go(), sx_async_ecjpake_verify_zkp_end() for an asynchronous version static inline int sx_ecjpake_verify_zkp( const struct sx_pk_ecurve curve, const struct sx_pk_point v, const struct sx_pk_point x, const sx_op r, const sx_op h, const struct sx_pk_point g ) { uint32_t status; struct sx_pk_dreq pkreq; pkreq = sx_ecjpake_verify_zkp_go(curve, v, x, r, h, g); if (pkreq.status) return pkreq.status; status = sx_pk_wait(pkreq.req); sx_ecjpake_verify_zkp_end(pkreq.req); return status; }
Asynchronous EC J-PAKE 3 point addition
Start a EC J-PAKE 3 point addition operation on the accelerator and return immediately. @remark When the operation finishes on the accelerator, call sx_ecjpake_3pt_add_end()
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
a Point on the curve
Parameters
b Point on the curve
Parameters
c Point on the curve Truncation or padding should be done by user application @return Acquired acceleration request for this operation static inline struct sx_pk_dreq sx_ecjpake_3pt_add_go( const struct sx_pk_ecurve curve, const struct sx_pk_point a, const struct sx_pk_point b, const struct sx_pk_point c) { struct sx_pk_dreq pkreq; struct sx_pk_inops_ecjpake_3pt_add inputs; pkreq = sx_pk_acquire_req(curve->cnx, SX_PK_CMD_ECJPAKE_3PT_ADD); if (pkreq.status) return pkreq; pkreq.status = sx_pk_list_ecc_inslots(pkreq.req, curve, 0, (struct sx_pk_slot )&inputs); if (pkreq.status) return pkreq; int opsz = sx_pk_get_opsize(pkreq.req); sx_pk_op2mem(b->x, inputs.x2_1.addr, opsz); sx_pk_op2mem(b->y, inputs.x2_2.addr, opsz); sx_pk_op2mem(c->x, inputs.x3_1.addr, opsz); sx_pk_op2mem(c->y, inputs.x3_2.addr, opsz); sx_pk_op2mem(a->x, inputs.x1_1.addr, opsz); sx_pk_op2mem(a->y, inputs.x1_2.addr, opsz); sx_pk_run(pkreq.req); return pkreq; }
Finish asynchronous (non-blocking) EC J-PAKE 3 point addition.
Finishes the EC J-PAKE 3 point addition and releases the reserved resources. @pre The operation on the accelerator must be finished before calling this function.
Parameters
req The previously acquired acceleration request for this operation
Parameters
gb The addition result static inline void sx_ecjpake_3pt_add_end( sx_pk_accel req, struct sx_pk_point gb ) { sx_async_finish_pair(req, gb->x, gb->y); }
Synchronous EC J-PAKE 3 point addition
Start a EC J-PAKE 3 point addition operation on the accelerator and return immediately. The 3 point addition operation has the following steps: 1. gb = a + b + c @remark When the operation finishes on the accelerator, call sx_ecjpake_3pt_add_end()
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
a Point on the curve
Parameters
b Point on the curve
Parameters
c Point on the curve
Parameters
gb The addition result Truncation or padding should be done by user application @return ::SX_OK @return ::SX_ERR_INVALID_SIGNATURE @return ::SX_ERR_OUT_OF_RANGE @return ::SX_ERR_POINT_NOT_ON_CURVE @return ::SX_ERR_NOT_INVERTIBLE @return ::SX_ERR_UNKNOWN_ERROR @return ::SX_ERR_BUSY @return ::SX_ERR_NOT_IMPLEMENTED @return ::SX_ERR_OPERAND_TOO_LARGE @return ::SX_ERR_PLATFORM_ERROR @return ::SX_ERR_EXPIRED @see sx_async_ecjpake_verify_zkp_go(), sx_async_ecjpake_verify_zkp_end() for an asynchronous version static inline int sx_ecjpake_3pt_add( const struct sx_pk_ecurve curve, const struct sx_pk_point a, const struct sx_pk_point b, const struct sx_pk_point c, struct sx_pk_point gb ) { uint32_t status; struct sx_pk_dreq pkreq; pkreq = sx_ecjpake_3pt_add_go(curve, a,b,c); if (pkreq.status) return pkreq.status; status = sx_pk_wait(pkreq.req); sx_ecjpake_3pt_add_end(pkreq.req, gb); return status; }
Asynchronous EC J-PAKE session key generation
Start a EC J-PAKE session key generation operation on the accelerator and return immediately. @remark When the operation finishes on the accelerator, call sx_ecjpake_gen_sess_key_end()
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
x4 Point on the curve
Parameters
b Point on the curve
Parameters
x2 Generated random number
Parameters
x2s (x2 s) % n Truncation or padding should be done by user application @return Acquired acceleration request for this operation static inline struct sx_pk_dreq sx_ecjpake_gen_sess_key_go( const struct sx_pk_ecurve curve, const struct sx_pk_point x4, const struct sx_pk_point b, const sx_op x2, const sx_op x2s) { struct sx_pk_dreq pkreq; struct sx_pk_inops_ecjpake_gen_sess_key inputs; pkreq = sx_pk_acquire_req(curve->cnx, SX_PK_CMD_ECJPAKE_GEN_SESS_KEY); if (pkreq.status) return pkreq; pkreq.status = sx_pk_list_ecc_inslots(pkreq.req, curve, 0, (struct sx_pk_slot )&inputs); if (pkreq.status) return pkreq; int opsz = sx_pk_get_opsize(pkreq.req); sx_pk_op2mem(x4->x, inputs.x4_1.addr, opsz); sx_pk_op2mem(x4->y, inputs.x4_2.addr, opsz); sx_pk_op2mem(b->x, inputs.b_1.addr, opsz); sx_pk_op2mem(b->y, inputs.b_2.addr, opsz); sx_pk_op2mem(x2, inputs.x2.addr, opsz); sx_pk_op2mem(x2s, inputs.x2s.addr, opsz); sx_pk_run(pkreq.req); return pkreq; }
Finish asynchronous (non-blocking) EC J-PAKE session key generation
Finishes the EC J-PAKE session key generation operation and releases the reserved resources. @pre The operation on the accelerator must be finished before calling this function.
Parameters
req The previously acquired acceleration request for this operation
Parameters
t The result static inline void sx_ecjpake_gen_sess_key_end( sx_pk_accel req, struct sx_pk_point t) { sx_async_finish_pair(req, t->x, t->y); }
Synchronous EC J-PAKE session key generation
Start a EC J-PAKE session key generation operation on the accelerator and return immediately. The session key generation has the following steps: | Param | Description | |:----- |:----------- |
| 1. T = (b | (x4 x2s)) x2 @remark When the operation finishes on the accelerator, call sx_ecjpake_gen_sess_key_end()
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
x4 Point on the curve
Parameters
b Point on the curve
Parameters
x2 Generated random number
Parameters
x2s x2 password
Parameters
t result Truncation or padding should be done by user application @return ::SX_OK @return ::SX_ERR_INVALID_SIGNATURE @return ::SX_ERR_OUT_OF_RANGE @return ::SX_ERR_POINT_NOT_ON_CURVE @return ::SX_ERR_NOT_INVERTIBLE @return ::SX_ERR_UNKNOWN_ERROR @return ::SX_ERR_BUSY @return ::SX_ERR_NOT_IMPLEMENTED @return ::SX_ERR_OPERAND_TOO_LARGE @return ::SX_ERR_PLATFORM_ERROR @return ::SX_ERR_EXPIRED @see sx_async_ecjpake_gen_sess_key_go(), sx_async_ecjpake_gen_sess_key_end() for an asynchronous version static inline int sx_ecjpake_gen_sess_key( const struct sx_pk_ecurve curve, const struct sx_pk_point x4, const struct sx_pk_point b, const sx_op x2, const sx_op x2s, struct sx_pk_point t ) { uint32_t status; struct sx_pk_dreq pkreq; pkreq = sx_ecjpake_gen_sess_key_go(curve, x4, b, x2, x2s); if (pkreq.status) return pkreq.status; status = sx_pk_wait(pkreq.req); sx_ecjpake_gen_sess_key_end(pkreq.req, t); return status; }
Asynchronous EC J-PAKE step 2 calculation
Start an EC J-PAKE step 2 calculation operation on the accelerator and return immediately. @remark When the operation finishes on the accelerator, call sx_ecjpake_gen_step_2_end()
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
x4 Point on the curve
Parameters
x3 Point on the curve
Parameters
x1 Point on the curve
Parameters
x2s (x2 s) % n
Parameters
s password Truncation or padding should be done by user application @return Acquired acceleration request for this operation static inline struct sx_pk_dreq sx_ecjpake_gen_step_2_go( const struct sx_pk_ecurve curve, const struct sx_pk_point x4, const struct sx_pk_point x3, const struct sx_pk_point x1, const sx_op x2s, const sx_op s) { struct sx_pk_dreq pkreq; struct sx_pk_inops_ecjpake_gen_step_2 inputs; pkreq = sx_pk_acquire_req(curve->cnx, SX_PK_CMD_ECJPAKE_GEN_STEP_2); if (pkreq.status) return pkreq; pkreq.status = sx_pk_list_ecc_inslots(pkreq.req, curve, 0, (struct sx_pk_slot )&inputs); if (pkreq.status) return pkreq; int opsz = sx_pk_get_opsize(pkreq.req); sx_pk_op2mem(x4->x, inputs.x4_1.addr, opsz); sx_pk_op2mem(x4->y, inputs.x4_2.addr, opsz); sx_pk_op2mem(x3->x, inputs.x3_1.addr, opsz); sx_pk_op2mem(x3->y, inputs.x3_2.addr, opsz); sx_pk_op2mem(x1->x, inputs.x1_1.addr, opsz); sx_pk_op2mem(x1->y, inputs.x1_2.addr, opsz); sx_pk_op2mem(x2s, inputs.x2s.addr, opsz); sx_pk_op2mem(s, inputs.s.addr, opsz); sx_pk_run(pkreq.req); return pkreq; }
Finish an asynchronous (non-blocking) EC J-PAKE step 2 calculation
Finishes the EC J-PAKE step 2 calculation operation and releases the reserved resources. @pre The operation on the accelerator must be finished before calling this function.
Parameters
req The previously acquired acceleration request for this operation
Parameters
a Point on the curve
Parameters
x2s Generated random password
Parameters
ga Point on the curve static inline void sx_ecjpake_gen_step_2_end( sx_pk_accel req, struct sx_pk_point a, sx_op x2s, struct sx_pk_point ga) { sx_op results = { a->x, a->y, x2s, ga->x, ga->y }; sx_async_finish_any(req, results, 5); }
Synchronous EC J-PAKE step 2 calculation
Start an EC J-PAKE step 2 calculation operation on the accelerator and return immediately. The step 2 calculation has the following steps: 1. ga = x1 + x3 + x4 2. rx2s = (x2s s) % curve.n 3. a = ga rx2s
Parameters
curve Elliptic curve on which to perform the operation.
Parameters
x4 Point on the curve
Parameters
x3 Point on the curve
Parameters
x1 Point on the curve
Parameters
x2s Generated random password
Parameters
s Password
Parameters
a Point on the curve
Parameters
rx2s Generated random password
Parameters
ga Point on the curve Truncation or padding should be done by user application @return ::SX_OK @return ::SX_ERR_INVALID_SIGNATURE @return ::SX_ERR_OUT_OF_RANGE @return ::SX_ERR_POINT_NOT_ON_CURVE @return ::SX_ERR_NOT_INVERTIBLE @return ::SX_ERR_UNKNOWN_ERROR @return ::SX_ERR_BUSY @return ::SX_ERR_NOT_IMPLEMENTED @return ::SX_ERR_OPERAND_TOO_LARGE @return ::SX_ERR_PLATFORM_ERROR @return ::SX_ERR_EXPIRED @see sx_async_ecjpake_gen_step_2_go(), sx_async_ecjpake_gen_step_2_end() for an asynchronous version static inline int sx_ecjpake_gen_step_2( const struct sx_pk_ecurve curve, const struct sx_pk_point x4, const struct sx_pk_point x3, const struct sx_pk_point x1, const sx_op x2s, const sx_op s, struct sx_pk_point a, sx_op rx2s, struct sx_pk_point ga ) { uint32_t status; struct sx_pk_dreq pkreq; pkreq = sx_ecjpake_gen_step_2_go(curve, x4, x3, x1, x2s, s); if (pkreq.status) return pkreq.status; status = sx_pk_wait(pkreq.req); sx_ecjpake_gen_step_2_end(pkreq.req, a, rx2s, ga); return status; }}