1.2.1.1.2.16 SilexPK status codes
@file
SX_PK_STATUSCODES_HEADER_FILE Macro
C
#define SX_PK_STATUSCODES_HEADER_FILE
/ Copyright (c) 2018-2020 Silex Insight sa Copyright (c) 2018-2020 Beerten Engineering scs SPDX-License-Identifier: BSD-3-Clause
SX_ERR_IK_MODE Function
C
#define SX_ERR_IK_MODE 16
@addtogroup SX_PK_STATUS
@{
The function or operation succeeded */
The function or operation was given an invalid parameter */
SX_ERR_INVALID_PARAM Macro
C
#define SX_ERR_INVALID_PARAM 1
Unknown error */
The operation is still executing */
SX_ERR_BUSY Macro
C
#define SX_ERR_BUSY 3
The input operand is not a quadratic residue */
The input value for Rabin-Miller test is a composite value */
SX_ERR_COMPOSITE_VALUE Macro
C
#define SX_ERR_COMPOSITE_VALUE 5
Inversion of non-invertible value */
The signature is not valid
SX_ERR_INVALID_SIGNATURE Macro
C
#define SX_ERR_INVALID_SIGNATURE 7
This error can happen during signature generation and signature verification
The functionality or operation is not supported */
The output operand is a point at infinity */
SX_ERR_POINT_AT_INFINITY Macro
C
#define SX_ERR_POINT_AT_INFINITY 9
The input value is outside the expected range */
The modulus has an unexpected value
SX_ERR_INVALID_MODULUS Macro
C
#define SX_ERR_INVALID_MODULUS 11
This error happens when the modulus is zero or even when odd modulus is expected
The input point is not on the defined elliptic curve */
The input operand is too large */
SX_ERR_OPERAND_TOO_LARGE Macro
C
#define SX_ERR_OPERAND_TOO_LARGE 13
A platform specific error */
The evaluation period for the product expired */
SX_ERR_EXPIRED Macro
C
#define SX_ERR_EXPIRED 15
The hardware is still in IK mode
SX_ERR_IK_MODE Macro
C
#define SX_ERR_IK_MODE 16
This error happens when a normal operation is started and the hardware is still in IK mode. Run command ::SX_PK_CMD_IK_EXIT to exit the IK mode and to run normal operations again
The parameters of the elliptic curve are not valid. */
Return a brief text string describing the given status code.
char Typedef
C
typedef const char (FUNC_SX_DESCRIBE_STATUSCODE)(int code);
SX_DESCRIBE_STATUSCODE Macro
C
#define SX_DESCRIBE_STATUSCODE ((FUNC_SX_DESCRIBE_STATUSCODE)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_DESCRIBE_STATUSCODE)))
Parameters
code Value of status code @return Text string describing the status code