1.2.1.1.2.14 Simpler functions for base Montgomery elliptic curve operations
@file
MONTGOMERY_HEADER_FILE Macro
C
#define MONTGOMERY_HEADER_FILE
/ Copyright (c) 2018-2020 Silex Insight sa Copyright (c) 2018-2020 Beerten Engineering scs SPDX-License-Identifier: BSD-3-Clause
Size in bytes of a point on X25519 curve */
Size in bytes of a point on X448 curve */
SX_X448_PT_SZ Macro
C
#define SX_X448_PT_SZ 56
@addtogroup SX_PK_MONT
@{
An X25519 point */
struct sx_x25519_pt {
Bytes array representation of a X25519 point **/
char bytes; };
An X448 point */
struct sx_x448_pt {
Bytes array representation of a X448 point **/
char bytes; };
Montgomery point multiplication (X25519)
SX_X25519_PTMULT Macro
C
typedef int (FUNC_SX_X25519_PTMULT)(struct sx_pk_cnx cnx, const struct sx_x25519_pt k, const struct sx_x25519_pt pt, struct sx_x25519_pt r); #define SX_X25519_PTMULT ((FUNC_SX_X25519_PTMULT)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_X25519_PTMULT)))
Compute r = pt k
The operands must be decoded and clamped as defined in specifications for X25519 and X448.
Parameters
cnx Connection structure obtained through SX_PK_OPEN() at startup
Parameters
k Scalar
Parameters
pt Point on the X25519 curve
Parameters
r Multiplication result of k and pt @return ::SX_OK @return ::SX_ERR_INVALID_PARAM @return ::SX_ERR_UNKNOWN_ERROR @return ::SX_ERR_BUSY @return ::SX_ERR_NOT_IMPLEMENTED @return ::SX_ERR_OPERAND_TOO_LARGE @return ::SX_ERR_PLATFORM_ERROR @return ::SX_ERR_EXPIRED @see SX_ASYNC_X25519_PTMULT_GO() and SX_ASYNC_X25519_PTMULT_END() for an asynchronous version
Asynchronous Montgomery point multiplication (X25519)
SX_ASYNC_X25519_PTMULT_GO Macro
C
typedef struct sx_pk_dreq (FUNC_SX_ASYNC_X25519_PTMULT_GO)(struct sx_pk_cnx cnx, const struct sx_x25519_pt k, const struct sx_x25519_pt pt); #define SX_ASYNC_X25519_PTMULT_GO ((FUNC_SX_ASYNC_X25519_PTMULT_GO)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_ASYNC_X25519_PTMULT_GO)))
Start a montgomery point multiplication on the accelerator and return immediately.
@remark When the operation finishes on the accelerator, call SX_ASYNC_X25519_PTMULT_END()
Parameters
cnx Connection structure obtained through SX_PK_OPEN() at startup
Parameters
k Scalar
Parameters
pt Point on the X25519 curve @return Acquired acceleration request for this operation @see SX_ASYNC_X25519_PTMULT_END() and SX_X25519_PTMULT()
Collect the result of asynchronous Montgomery point multiplication (X25519)
SX_ASYNC_X25519_PTMULT_END Macro
C
typedef void (FUNC_SX_ASYNC_X25519_PTMULT_END)(sx_pk_accel req, struct sx_x25519_pt r); #define SX_ASYNC_X25519_PTMULT_END ((FUNC_SX_ASYNC_X25519_PTMULT_END)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_ASYNC_X25519_PTMULT_END)))
Get the output operand of the Montgomery point multiplication and release accelerator.
@remark The operation on the accelerator must be finished before calling this function.
Parameters
req The previously acquired acceleration request for this operation
Parameters
r Multiplication result of k and pt @see SX_ASYNC_X25519_PTMULT_GO() and sx_async_x25519_ptmult()
Montgomery point multiplication (X448)
SX_X448_PTMULT Macro
C
typedef int (FUNC_SX_X448_PTMULT)(struct sx_pk_cnx cnx, const struct sx_x448_pt k, const struct sx_x448_pt pt, struct sx_x448_pt r); #define SX_X448_PTMULT ((FUNC_SX_X448_PTMULT)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_X448_PTMULT)))
Compute r = pt k
The operands must be decoded and clamped as defined in specifications for X25519 and X448.
Parameters
cnx Connection structure obtained through SX_PK_OPEN() at startup
Parameters
k Scalar
Parameters
pt Point on the X448 curve
Parameters
r Multiplication result of k and pt @return ::SX_OK @return ::SX_ERR_INVALID_PARAM @return ::SX_ERR_UNKNOWN_ERROR @return ::SX_ERR_BUSY @return ::SX_ERR_NOT_IMPLEMENTED @return ::SX_ERR_OPERAND_TOO_LARGE @return ::SX_ERR_PLATFORM_ERROR @return ::SX_ERR_EXPIRED @see SX_ASYNC_X448_PTMULT_GO() and SX_ASYNC_X448_PTMULT_END() for an asynchronous version
Asynchronous Montgomery point multiplication (X448)
SX_ASYNC_X448_PTMULT_GO Macro
C
typedef struct sx_pk_dreq (FUNC_SX_ASYNC_X448_PTMULT_GO)(struct sx_pk_cnx cnx, const struct sx_x448_pt k, const struct sx_x448_pt pt); #define SX_ASYNC_X448_PTMULT_GO ((FUNC_SX_ASYNC_X448_PTMULT_GO)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_ASYNC_X448_PTMULT_GO)))
Start a montgomery point multiplication on the accelerator and return immediately.
@remark When the operation finishes on the accelerator, call SX_ASYNC_X448_PTMULT_END()
Parameters
cnx Connection structure obtained through SX_PK_OPEN() at startup
Parameters
k Scalar
Parameters
pt Point on the X448 curve @return Acquired acceleration request for this operation @see SX_ASYNC_X448_PTMULT_END() and SX_X448_PTMULT()
Collect the result of asynchronous Montgomery point multiplication (X448)
SX_ASYNC_X448_PTMULT_END Macro
C
typedef void (FUNC_SX_ASYNC_X448_PTMULT_END)(sx_pk_accel req, struct sx_x448_pt r); #define SX_ASYNC_X448_PTMULT_END ((FUNC_SX_ASYNC_X448_PTMULT_END)((uint32_t )(API_TABLE_BASE_ADDRESS + ATO_SX_ASYNC_X448_PTMULT_END)))
Get the output operand of the Montgomery point multiplication and release the reserved resources.
@remark The operation on the accelerator must be finished before calling this function.
Parameters
req The previously acquired acceleration request for this operation
Parameters
r Multiplication result of k and pt @see SX_ASYNC_X448_PTMULT_GO() and sx_async_x448_ptmult()
}