Message Authentication Code AES CMAC.
CMAC_API_FILE Macro
C
#define CMAC_API_FILE
@file @copyright Copyright (c) 2020 Silex Insight. All Rights reserved.
Examples: The following examples show typical sequences of function calls for generating a mac. @code
- One-shot operation MAC generation SX_MAC_CREATE_AESCMAC(ctx, ...) SX_MAC_FEED(ctx, ...) SX_MAC_GENERATE(ctx) SX_MAC_WAIT(ctx) @endcode
Prepares an AES CMAC generation.
This function initializes the user allocated object \p c with a new AES CMAC operation context needed to run the CMAC generation.
After successful execution of this function, the context \p c can be passed to any of the CMAC functions.
Parameters
c CMAC operation context
Parameters
key key used for the CMAC generation operation, expected size 16, 24 or 32 bytes @return ::SX_OK @return ::SX_ERR_INVALID_KEYREF @return ::SX_ERR_INVALID_KEY_SZ @return ::SX_ERR_INCOMPATIBLE_HW @return ::SX_ERR_RETRY | Param | Description | |:----- |:----------- |
| @pre | key reference provided by \p key must be initialized using SX_KEYREF_LOAD_MATERIAL() or SX_KEYREF_LOAD_BY_ID()