3.1 MPLAB® X IPE HUT Code Programming Process with In-Circuit Serial Programming™ Header
In this demonstration, the user must program the PIC32MZ1025W1 with the HUT firmware using the PC with the MPLAB X IPE.
Note: The user must perform the HUT firmware programming before proceeding with the rest of the operation with the MCHPRT3 tool.
The In-Circuit Serial Programming (ICSP™) header (J206) is a standard six pin staggered header. The J206 allows in-circuit emulation, debugging using Microchip’s in-circuit emulator tools and also allows direct programming of the WFI32E01 module. The ICSP header supports external debuggers, such as MPLAB PICkit™ 4 and MPLAB Snap. Use the standard ICSP header to connect an MPLAB programmer or debugger to the PIC32 WFI32E Curiosity
Board. The following figure illustrates the connection between the ICSP header, external debuggers and the PIC32 WFI32E Curiosity
Board.The following figure illustrates the start-up window of the MPLAB X IPE tool. Perform the following steps to set up the HUT firmware programming:
- Set up the connection between the PIC32 WFI32E Curiosity Board and PC. For more details, refer to Getting Started with MCHPRT3 Tool GUI for PIC32MZ1025W1.
- Start the MPLAB X IPE tool, and select PIC32MZ1025W104132 from the “Device” field.
- Click Connect to connect the PIC32 WFI32E Curiosity Board to the MPLAB X IPE tool for the HUT firmware programming. If the device name is not available, check the USB connection (step 1).
- Click Browse to load the HUT firmware HEX file (see Table 2-2).
Figure 3-2. Start-Up Window of the MPLAB X IPE Tool - Click Program
.
- After the completion of the HUT firmware programming, click Disconnect to disconnect the PIC32 WFI32E Curiosity
Board and MPLAB X IPE tool (see the following figure).
Figure 3-3. MPLAB X IPE – Programming Complete
Disconnect external debuggers (MPLAB PICkit 4 or MPLAB Snap) and Reset PIC32 WFI32E Curiosity Board for the RF test using the MCHPRT3 tool.