20.1.3 Signal Routing Port Output and Data Register
The output of the Signal Routing Port is available through the RWn virtual pins. The status of these Signal Routing pins can be read using the PORTW data register.
PORTW is a bidirectional port register. However, unlike a typical I/O port, PORTW consists of
two different registers internally which are not user-accessible – ‘PORTW read’ and ‘PORTW write’
registers as shown in Figure 20-1. Reading from the PORTW register returns result from the ‘PORTW read’ register, which reads
the selected Signal Routing Port input (as per PORTWINx selection). Writing to the PORTW register writes to the ‘PORTW write’ register,
which is the actual data register. While the PORTW register can be read any time, writes to the
PORTW register can only happen when the clock to the module is disabled (PWCLKEN = 0).
The ‘PORTW write’ register is enabled using DFn bits in the PORTWDF register. The PORTWDF register controls whether the Signal Routing Port input is connected to the flip-flop (data register) or not. When enabled, the input from the PORTWINx selection is routed through the ‘PORTW write’ register (data register) to the output. When disabled, the Signal Routing Port input is directly connected to the output, thus creating a completely asynchronous path between the input and output of the Signal Routing Port. Each bit in the PORTWDF register can individually enable/disable the flip-flop for each bit in the Signal Routing Port. See Figure 20-1 for details.
Unlike a typical I/O port, the ‘PORTW write’ register can be clocked by various clock sources.
Refer to the Signal Routing Port Clock section for more details. When the clock to the module is disabled
(PWCLKEN = 0), the ‘PORTW write’ register is clocked using the instruction clock
(FOSC/4), which allows PORTW write operations in software. This allows software to
initialize the state of a Signal Routing pin before the clock is enabled. When the module clock is
enabled (PWCLKEN = 1), the ‘PORTW write’ register is clocked using the clock input
from the PORTWCLK register selection. This prevents any software writes to the ‘PORTW write’ register
(data register). In this case, the ‘PORTW write’ register can only be written through the Signal
Routing Port input from PORTWINx register selection. This allows the formation of hardware-based
state machines by interconnecting multiple core independent peripherals through a flip-flop to the
output using a specific clock.
In addition to the ‘PORTW read’ register, the Signal Routing Port outputs (RWn Signal Routing pins) are also routed through PPS and are available for use by other modules as PPS inputs. See the “PPS Inputs” section in the “PPS – Peripheral Pin Select Module” chapter for more information.
- Reading PORTW from ‘PORTW read’ register reads the value of the ‘PORTW write’ data register only when the flip-flop is enabled for the corresponding bit using the PORTWDF register. If the flip-flop is disabled, an asynchronous path is created and ‘PORTW read’ reads the unlatched value as per the PORTWINx input selection.
- There must be one instruction cycle delay between write and read of the PORTW register, otherwise the previously written value will be read. This is because it takes one clock for the data to be latched from the ‘PORTW write’ register to the ‘PORTW read’ register.