36.4.2.6 Stop Condition Timing
A Stop condition occurs when SDA transitions from an Active state to an Idle state while SCL is
Idle. Host hardware will issue a Stop condition when it has completed its current
transmission and is ready to release control of the bus. A Stop condition is also issued
after an error condition occurs, such as a bus time-out or when a NACK condition is
detected on the bus. User software may also generate a Stop condition by setting the
Stop (P)
bit.
After the ACK/NACK sequence of the final byte of the
transmitted/received packet, hardware pulls SCL low for half of an SCL period
(TSCL/2) (see the figure below). After the half SCL period, hardware
releases SCL and then samples SCL to ensure it is in an Idle state (SCL =
1). Host hardware then waits the duration of the Stop condition
setup time (TSU:STO) and releases SDA, setting the Stop Condition Interrupt
Flag (PCIF).
If the Stop Condition Interrupt Enable (PCIE)
bit is also set, the generic I2CxIF is also set. Important: At least one SCL low
period must appear before a Stop condition is valid. If the SDA line transitions low and
then high again while SCL is high, the Stop condition is ignored, and a Start condition
will be detected by the receiver.
Important:
- At least one SCL low period must appear before a Stop is valid.
- See the device data sheet electrical specifications for Stop condition setup and hold times.