13.8 Scanning Modes
The interaction of the scanner with the system operation is controlled by the priority
selection in the system arbiter (refer to the “Memory Access Scheme” section for
more details). When using the scanner module in conjunction with the CRC module, the
system arbiter needs to be configured such that the scanner has a higher priority than
the CPU to ensure that a memory access request is granted when it occurs. Additionally,
BURSTMD
and TRIGEN
bits also determine the operation of the scanner.