18.6.3 Clock Failure Detection Operation
The Clock Failure Detector (CFD) allows the user to monitor the external clock or crystal oscillator clock signal provided by the External Multipurpose Crystal Oscillator (XOSC). It detects failing operation of the XOSC clock and allows to switch to a safe clock in case of clock failure. The safe clock is derived from the DFLL48M with a configurable prescaler. The user can also switch from the safe clock to the XOSC clock in case of clock recovery. This allows to configure the safe clock in order to fulfill the operative conditions of the microcontroller. The CFD operation is automatically suspended when the XOSC clock is not requested in ONDEMAND mode or halted in STANDBY.
The user interface registers allow to enable, disable and configure the CFD. The Status register gives status on failure and clock switch conditions. The Clock Failure Detector can optionally trigger an interrupt or an event when a failure is detected.
Clock Failure Detection
At reset, the CFD is disabled. The CFD does not monitor the XOSC clock when the oscillator is disabled (XOSCCTRLA.ENABLE = 0).
Before starting the CFD operation, the user must start and enable the safe clock source (DFLL48M). To start the CFD operation, the user must write a one to the CFD Enable bit in the External Oscillator Control register (XOSCCTRLA.CFDEN). After the start or restart of the XOSC, the CFD does not detect failure until the start-up time, as configured by the Oscillator Start-Up Time (XOSCCTRLA.STARTUP) in the External Multipurpose Crystal Oscillator Control register, is elapsed. Once the XOSC Start-Up Time is elapsed, the XOSC clock is constantly monitored.
During a period of 4 safe clocks , the CFD watches for a clock activity from the XOSC. There must be one rising and one falling XOSC clock edges during a 4 safe clock periods to meet a non-failure status. If no activity is detected, the failure status is asserted. The Clock Failure status bit in the Status register (STATUS.CLKFAIL) is set. The Clock Failure interrupt flag bit in the Interrupt Flag register (INTFLAG.CLKFAIL) is set. If the CLKFAIL bit in the Interrupt Enable Set register (INTENSET.CLKFAIL) is set, an interrupt is generated . An output event is generated as well, if the Event Output enable bit in the Event Control register (EVCTRL.CFDEO) is set.
The XOSC clock continues to be monitored after a clock failure. The Clock Failure status bit in the Status register (STATUS.CLKFAIL) reflects the current XOSC clock activity.
Clock Switch Back
When a clock failure is detected, the XOSC clock is replaced by the safe clock in order to maintain an active clock during the XOSC clock failure. The safe clock source can be downscaled with a configurable prescaler to ensure that the safe clock frequency does not exceed the operating conditions selected by the application. When the XOSC clock is switched to the safe clock, the Clock Switch bit (STATUS.XOSCCKSW) in the Status register is set.
When the XOSC clock is switched to the safe clock, the External Multipurpose Crystal Oscillator Ready bit in the Status register (STATUS.XOSCRDY) is set when the safe clock is stable and ready to be used as a clock source.
When the CFD has switched to the safe clock, the XOSC is not disabled. The application must take the necessary actions to disable the oscillator. The application must also take the necessary actions to configure the system clocks to continue normal operations.
In the case the application can recover the XOSC, the Clock Failure status bit in the Status register (STATUS.CLKFAIL) is cleared. The application can switch back to the XOSC clock by writing a one to Switch Back bit (XOSCCTRLA.SWBEN) in the External Oscillator Control register. Once the XOSC clock is switched back, the Switch Back bit (XOSCCTRLA.SWBEN) is cleared by the hardware.
If the switch back can not complete due to a persistent failure, it will prevent the system from entering into low power sleep mode.
To stop the clock request the user can disable the XOSC (XOSCCTRLA.ENABLE=0) and disable the CFD detection (XOSCCTRLA.CFDEN=0).
Prescaler:
The CFD has an internal configurable prescaler (XOSCCTRLA.CFDPRESC) to generate the safe clock from the DFLL48M clock. The prescaler size allows to scale down the DFLL48M clock such that the safe clock is not higher than the XOSC clock frequency monitored by the CFD. The frequency divider is 2^CFDPRESC where CFDPRESC range from 0 to 15.
Example: for an external crystal oscillator at 8 MHz and the DFLL48M internal oscillator configured to generate a 48 MHz clock, the prescaler must select a downscale value above 6 (48/8), for example, 8, therefore CFDPRESC = 3.
Event:
If the Event Output enable bit in the Event Control register (EVCTRL.CFDEO) is set, the CFD clock failure will be output on the Event Output. When the CFD is switched to the safe clock, the CFD clock failure will not be output on the Event Output.
Sleep Mode:
The CFD is halted depending on configuration of the XOSC and the peripheral clock request. For further details, refer to the Sleep Behavior table. The CFD interrupt can be used to wake up the device from sleep modes.
- PLL0 must be stepped down in ≦ 75 MHz increments to ≦ 75 MHz output when entering sleep modes.
- PLL0 must be stepped up to the operating frequency in ≦ 75 MHz increments after exiting sleep modes.
- The step delay for both of these processes needs to be ≧ 1 us.