34.11.3.4 Events

The PORT allows input events to control individual I/O pins. These input events are generated by the EVSYS module and can originate from a different clock domain than the PORT module.

The PORT can perform the following actions:

  • Output (OUT): The I/O pin will be set when the incoming event has a high level ('1') and cleared when the incoming event has a low-level ('0').
  • Set (SET): The I/O pin will be set when an incoming event is detected.
  • Clear (CLR): The I/O pin will be cleared when an incoming event is detected.
  • Toggle (TGL): The I/O pin will toggle when an incoming event is detected.

The event is output to pin without any internal latency. For SET, CLR, and TGL event actions, the action will be executed up to three clock cycles after a rising edge.

Note: When an application has critical timing requirements, continuous sampling mode must be enabled.

The event actions can be configured with the Event Action m bit group in the Event Input Control register (EVCTRL.EVACTm). Writing a '1' to a PORT Event Enable Input m of the Event Control register (EVCTRL.PORTEIm) enables the corresponding action on input event. Writing '0' to this bit disables the corresponding action on input event. Note that several actions can be enabled for incoming events. If several events are connected to the peripheral, any enabled action will be taken for any of the incoming events. Refer to the Event System (EVSYS) for additional information on configuring the Event System.

Each event input can address one I/O pin at a time. The selection of the pin is indicated by the PORT Event Pin Identifier of the Event Input Control register (EVCTR.PIDn). On the other hand, one I/O pin can be addressed by up to four different input events. To avoid action conflict on the output value of the register (OUT) of this particular I/O pin, only one action is performed according to the table below.

Note that the following truth table can be applied to any SET/CLR/TGL configuration from two to four active input events.

Table 34-3. Priority on Simultaneous SET/CLR/TGL Event Actions
EVACT0EVACT1EVACT2EVACT3Executed Event Action
SETSETSETSETSET
CLRCLRCLRCLRCLR
All Other Combinations TGL

Exercise caution when the event is output to the pin. Due to the fact the events are received asynchronously, the I/O pin may have unpredictable levels, depending on the timing of when the events are received. When several events are output to the same pin, the lowest event line will get the access. All other events will be ignored.