3 Accessing RNBD451 Over UART
The most common application for the host MCU to control the RNBD451 module is via ASCII commands. For development and prototyping purposes, using a terminal emulator to send commands and data over UART is recommended. Any terminal emulator, such as TeraTerm (Windows®) or CoolTerm (Mac® OS X®), is used to control and configure the RNBD451 module via UART on the host PC.
With the RNBD451 module connected to a computer and a serial port enumerated for the UART port, run the terminal emulator to open the COM port using the port settings defined in the following table.
| UART Setting | Default Value |
|---|---|
| Baud rate | 115200 |
| Data bits | 8 |
| Parity | None |
| Stop bits | 1 |
| Flow control | Disabled |
To enter Command mode, type $$$ into the terminal emulator. When the RNBD451 module enters Command mode, the
RNBD451 module sends the string
CMD> via the UART to indicate the start of the Command
mode session.
When in Command mode, valid ASCII commands are issued to control or configure the RNBD451 module. All commands end with a
carriage return <cr>('\r', \x0d). Do not issue any
subsequent command until a response is received for the previous command.
For commands, AOK indicates a positive or successful response, whereas,
Err indicates an error or negative response. By default,
when the RNBD451 module is ready to
receive the next command, the command prompt CMD> is sent to
UART.
To return to Data mode, type ---<cr>. Also, in the connected and data
channel enabled state, the RNBD451 module
can enter into Data mode. For this, it is mandatory to have the UART transparent
feature enabled. For details on enabling the UART transparent feature, refer to
Default Service Configure (SS,<hex8>).
- The module supports
Fast Data mode. In this mode, the module does not enter Command
mode even if it receives
$$$. To enable Fast Data mode, use commandSR. For more details, refer to Set Application Options (SR,<hex16>). -
The RNBD451 module supports Low Power mode. If the RNBD451 module’s low power is enabled, the host MCU must wake up the RNBD451 module before sending the UART data out. To wake up the module, pull the UART RX indication pin (PB4) to low.