5.4.1.1 Set Appearance (SAPR,<hex16>)

Format: SAPR,<hex16>

This command sets the appearance of the RNBD451 module in the GAP service. It expects one 16-bit hex input parameter. Bluetooth SIG defines the appearance code for different devices. For more details, refer to the Appearance Values Bluetooth® Document (2021-11-24).

Default:0000
Example:SAPR,0340// Set appearance to Generic Heart Rate Sensor
Response:AOK// Success
Err// Syntax error or invalid parameter
Note: The PDS stores the parameter and is effective immediately without a reboot.