12 Document Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

RevisionDateSectionDescription
C07/2026ASCII Command InterfaceAdded note
UART Mode Switch (PB2)Added note
Updated the command names and command
C07/2026 Updated the command names and command
Set Proprietary Characteristics (SPC,<hex16/hex128>,<hex8>,<hex8>[,<hex8])Added note
Write Local Characteristic Value (SHW,<hex16>…)Added note
Write Local Characteristic Value for Multiple Links (SHWM,<hex16>…)Added note
Write Remote Characteristic Value for Multiple Links (CHWM,<hex16>,…)Updated bit values
B10/2023IntroductionMajor update
FeaturesMinor update
ASCII Command InterfaceMajor update
Transparent UARTMajor update
Custom/SIG Defined GATT ServicesMajor update
Acronyms and AbbreviationsFew new acronyms added
PTA FunctionNew topic
Command ReferenceMajor update
Command DetailsMinor update
System Configuration CommandsRemoved the description
Defining Multiple ServicesDeleted this topic
Set Service Configure (SSC,<hex8>)Minor update
Query Current Connection Status (QCCS)Major update
Set Enter Command Character (S$,<char>)Minor update
Enter/Exit Remote Command Mode (RMT,<0,1>[,<hex16> Connection Handle])Major update
Set Application Options (SAO,<hex16>[,<hex16>])Minor update
Set SW PTA (SPTA,<0,1>)Added new topic
B10/2023Get SW PTA Setting (GPTA)Added new topic
Set HCI (SHCI,<0,1>)Added new topic
Set Name with Address (SNA,<text>)Minor update
Set Device Name (SN,<text>)Minor update
Get Remote Device Name (GNR[,<hex16>])Minor update
Read Remote TX Power (MRTP,<hex16>,<hex8>)Minor update
Set RF Output Power (SGA,<0-8>/SGC,<0-8>)Added one more notes
Start Advertising (A[,<hex16>,<hex16>,…])Major update
Set Advertisement Data (IA/IS/NA/NS)Minor update
Set Extended Advertisement Data (IAE/NAE/ISE/NSE)Minor update
Set Fast Advertisement Parameter (STA, <hex16>,<hex16>,<hex16>)Added new topic
Set Beacon Data (IB/NB)Added new topic
Set Beacon Parameter (SBP,<hex16>) Added new topic
Get Beacon Parameter (GBP,<hex16>)Added new topic
Set Advertising Configuration (SAC,<0-2>) Added new topic
Get Advertising Configuration (GAC,<0-2>)Added new topic
Start Extended Bluetooth Low Energy Scanning (FE,<hex16>...)Major update
Set Initial Connection Parameter (SICP,<hex16>,<hex16>,<hex16>,<hex16>) Minor update
Update Connection Parameter (UCP,<hex16>,<hex16>,<hex16>,<hex16>[,<hex16>])Minor update
Connect Device with Extended Parameter (CE,<0,1>,<address>…)Minor update
Set PHY Preference (CSPHY,<hex16>…)Added one note
Set Remote Command Mode Password (SPW,<text>) Added new topic
Get Remote Command Mode Password (GPW)Added new topic
Set Firmware Version (SDF,<text>)Added one note
Set Model Name (SDM,<text>)Minor update
Write Local Characteristic Value (SHW,<hex16>…)Added notes
Write Local Characteristic Value for Multiple Links (SHWM,<hex16>…)Added new topic
Query as Client by Service (QCS[,<hex16 Connection Handle>])Minor update
Send Transparent Data (IE,<hex16>,<hex16>,<hex8>….)Minor update
Set Link Quality Indication (SLQI, <1/0>, <hex8>, <hex8>)Added default row
Set Battery Voltage Factors (SBVF,<hex16>,<hex8>)Added default row
Set PMU Mode (SPMU,<0,1>)Added default row
Set UART TX Indication (STI,<hex8>,<hex8>)Updated default value
DFU CommandsAdded new chapter
HCI ModeAdded new chapter
Deprecated CommandsMinor update
Command ResponseMinor update
RNBD451 Device Firmware Update ProcedureAdded new chapter
Appendix C: Command Summary Quick ReferenceAdded more commands
A01/2023DocumentInitial revision