5.3.1.1 Set Name with Address (SNA,<text>)
Format:
SNA,<text>
This command sets a serialized Bluetooth name for the device, where <text> is up to 15 alphanumeric characters. This command automatically appends the last two bytes of the Bluetooth MAC address along with _ (underscore) to the name, which is useful for generating a custom name with unique numbering. This command does not have a corresponding get command.
| Default: | N/A | |
| Example: | SNA,MyDevice | // Set the device name to MyDevice_XXXX |
| Response: | AOK | // Success |
Err | // Syntax error or invalid parameter | |
Note: This parameter is stored in PDS and is effective after restarting advertisement. | ||