5.7.3.1.5 OTAPC DFU Image Distribution
Format: DFUD <hex16>, <hex content>
Use the DFUD command for new image distribution. The payload length must be no larger than the max fragmented image size that the RNBD451 responded with in the DFUU command. When the DFUD command is called, no other DFU command is acceptable until completion of the update. This means DFUD can be successively called in several times and cannot be terminated before sending all of the image payload.
During the firmware distribution, if the timeout exceeds the maximum allowed timeout, the RNBD451 enters the Command mode.
| Example: | DFUD,0100, <hex> | // Update fragmented of FW image for length 0x100 |
| Response: | AOK | // Device received without error |
| Err | // State error, payload size error or command parameter error | |
| %DFU_TIMEOUT% | // The device responds with timeout status if the subsequent distribution command has not given an accepted timeout period |