During the firmware update, the below mentioned information will display on the tool.Figure 8-29. Microchip RNBD Utility Tool OTAPC Tab Remote Device Firmware Update in Progress
Progress label that displays the percentage of completion
Live Progress bar update view
Status label displays the current status
Total bytes completed
Background update station on console text view
After completion, the tool updates the following:
A message box displaying the DFU update completion. Press OK to proceed.
Progress indicator shows 100%
Status changes to DFU Update Completed!
Bytes completed matches with the total bytes
A Firmware Distribution Complete message on the console text logFigure 8-30. Microchip RNBD Utility Tool OTAPC Tab Remote Device Firmware Update Complete
A message box displays the DFU update completion. Press OK to proceed.
Progress indication shows 100%
Status changes to DFU Update Completed!
Bytes completed matches with the total bytes
A Firmware Distribution Complete message on the console text log
Upon pressing OK on the message box, the total time taken for the firmware update will be displayed on console text log.Figure 8-31. Microchip RNBD Utility Tool OTAPC Tab Remote Device Firmware Update Time Complete
DS50003467C
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.